SVD file for i.MX28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SVD file for i.MX28

1,819件の閲覧回数
alexlesuper
Contributor I

Hello,

I was wondering if the SVD XML file for the i.MX28 could be made available? I've tried looking on the ARM (https://cmsis.arm.com/vendor/freescale-semiconductor/ ) website and there are only MK device SVD files available. Having this file handy would greatly speed up my debugging and development process.

Thanks,

Alexandre Courtemanche

ラベル(2)
0 件の賞賛
返信
1 返信

1,660件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Alejexandre,

You are not going to find SVD file for the i.MX28 since it is an ARM926 Core, which means the only CMSIS-SVD files are for Cortex processors or Microcontrollers like the Kinetis family or the i.MX6 family.  In this case if you are using a DS-5 for debugging,  I think you only need to have the connection configuration using the proper script to initialize the device and that´s it.