SRC_GPR10[core1_ERROR_STATUS] clear

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRC_GPR10[core1_ERROR_STATUS] clear

Jump to solution
978 Views
Kazuma_Sasaki
Senior Contributor I

Please let me confirm SRC_GPR10[core1_ERROR_STATUS] behavior.

SRC_GPR10[core1_ERROR_STATUS] bit is set to 1b by the BOOT ROM during booting process on Core1.

I expected this bit automatically clear when happened error solved or after resetting core1.

However, SRC_GPR10[core1_ERROR_STATUS] bit has not cleared until writing 0 to this field.

<Question>

Q1. According to the RM described SRC_GPR10[core1_ERROR_STATUS] bit is read only as following figure. Is it right?
Q2. Should we clear SRC_GPR10[core1_ERROR_STATUS] field by our self? Do we need writing 0 to this field?

pastedImage_2.png

pastedImage_1.png

<My test result>

* I attached my test application. it is out-put "hello world" to check core1 boot completion.

1. Test app copy to the USB memory. then, the USB memory connect to the SABRE-AI board.

2. Input following command via U-BOOT prompt.

=> usb start

=> fatload usb 0 0x10000000 mp_debug.bin
=> md.l 0x20d8044 1
020d8044: 00000000 ....

*Set invalid entry point to SRC_GPR3 register. then, Core1 enable.

=> mw.l 0x20d8028 0x188006d0
=> mw.l 0x20d8000 0x00404520
=> md.l 0x20d8044 1
020d8044: 02000000

*SRC_GPR10[core1_ERROR_STATUS] occurred.

=> mw.l 0x20d8028 0x100006d0
=> mw.l 0x20d8000 0x00404520
=> ***** Hello World *****
md.l 0x20d8044 1
020d8044: 02000000 ....

*Set correct entry point to SRC_GPR3 register. then, Core1 reset.

*Test application is working without error. but, SRC_GPR10[core1_ERROR_STATUS] is remaining.

*Also, I tried warm-reset to clear SRC_GPR10[core1_ERROR_STATUS].

=> mw.l 0x20d8000 0x00400521
=> mw.l 0x20bc000 0x14

Resetting CPU ...

resetting ...


U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+ga57b13b (Jan 09 2018 - 22:04:27 +0800)

CPU: Freescale i.MX6DL rev1.1 at 792MHz
CPU: Commercial temperature grade (0C to 95C) at 50C
Reset cause: unknown reset
Board: MX6Q-Sabreauto revA
I2C: ready
DRAM: 2 GiB
PMIC: PFUZE100 ID=0x10
NAND: 0 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
=> md.l 0x20d8044 1
020d8044: 02000000 ....

* But, SRC_GPR10[core1_ERROR_STATUS] is remaining.

* Finally, I could clear this error by over-write 0b to this field.

=> mw.l 0x20d8044 0x00000000
=> md.l 0x20d8044 1
020d8044: 00000000 ....

Best Regards,

Kazuma Sasaki.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
885 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

this bit is used exclusively by ROM and since ROM sources are not available

for customers, no more details are available regarding this bit, sorry.

Please review below part of Reference Manual description below:

NOTE


This register is used by the ROM code and should not be used
by application software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
886 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

this bit is used exclusively by ROM and since ROM sources are not available

for customers, no more details are available regarding this bit, sorry.

Please review below part of Reference Manual description below:

NOTE


This register is used by the ROM code and should not be used
by application software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
885 Views
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

I see. Thank you for your support.

Best Regards,

Kazuma Sasaki

0 Kudos
Reply