SRAM using EIM in a iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SRAM using EIM in a iMX6

8,668件の閲覧回数
_andev_
Contributor II

Hi all,

We're connecting a 4MB Static RAM using the EIM interface in a custom iMX6 board.

We are trying to set a filesystem in that SRAM.

The kernel version is from yocto 3.10.53. We're only using the pins:

- EIM_CS0_B

- EIM_OE_B

- EIM_RW

- EIM_DATA00 to EIM_DATA15

- EIM_AD00 to EIM_ADDR21

and in DTS we have:

/*https://www.kernel.org/doc/Documentation/devicetree/bindings/bus/imx-weim.txt*/

&weim {

    pinctrl-names = "default";

    pinctrl-0 = <&pinctrl_weim_ram_1 &pinctrl_weim_cs0_1>;

    #address-cells = <2>;

    #size-cells = <1>;

    /* <cs-number> 0 <physical address of mapping> <size> = size 64MB -> addr=22 pins*/

    ranges = <0 0 0x08000000 0x008000000>;

    status = "okay";

    sram@0,0 {

        compatible = "mtd-ram";

        reg = <0 0 0x00400000>;

        #address-cells = <1>;

        #size-cells = <1>;

        bank-width = <2>;

        /* EIM_CSnGCR1, EIM_CSnGCR2, EIM_CSnRCR1, EIM_CSnRCR2, EIM_CSnWCR1, EIM_CSnWCR2 */

        fsl,weim-cs-timing = <0x403184B1 0x00001010 0x14017000

                0x00000000 0x14000E00 0x00000000>;

    };

};

I have three question:

1) To use the SRAM as a block device where we can set a filesystem the "mtd-ram" is the correct choice?

With the next command we can see the device recognized

# cat /proc/mtd

2) With that configuration we can see signals in the scope but if we try to make a fs in the block device related

we get an error. Is this correct?

# mkfs.ext2 /dev/mtdblock0

# mount /dev/mtdblock0 kk/

We have a SPI device too and the previous commands works ok.

3) Are there very obvious mistakes in this weim DTS definition we are not catching?

Any info is welcome, thanks!

0 件の賞賛
返信
8 返答(返信)

4,330件の閲覧回数
durmus
Contributor IV

Hi,

We have a SPI device too and the previous commands works ok.

Do you have an SPI SRAM device in your board? If so, could you please share

- which product it is

- what driver you are using

- device-tree entry

I would very much appreciate that.

Thank you.

0 件の賞賛
返信

4,331件の閲覧回数
_andev_
Contributor II

Hi,

- We have a M25P32

- driver: options in kernel

CONFIG_MTD_RAM=y

CONFIG_MTD_PHYSMAP_OF=y

CONFIG_MTD_M25P80=y

- device tree:

+&ecspi1 {

+    fsl,spi-num-chipselects = <1>;

+    cs-gpios = <&gpio3 19 0>;

+    pinctrl-names = "default";

+    pinctrl-0 = <&pinctrl_ecspi1_1>;

+    status = "okay";

+

+    flash: m25p32@0 {

+        #address-cells = <1>;

+        #size-cells = <1>;

+        compatible = "st,m25p32";

+        spi-max-frequency = <20000000>;

+        reg = <0>;

+    };

+};

+

+&weim {

+    pinctrl-names = "default";

+    pinctrl-0 = <&pinctrl_weim_ram_1 &pinctrl_weim_cs0_1>;

+    #address-cells = <2>;

+    #size-cells = <1>;

+    /* <cs-number> 0 <physical address of mapping> <size> = size 64MB -> addr=22 pins*/

+    ranges = <0 0 0x08000000 0x008000000>;

+    status = "okay";

+

+    sram@0,0 {

+        compatible = "mtd-ram";

+        reg = <0 0 0x00400000>;

+        #address-cells = <1>;

+        #size-cells = <1>;

+        bank-width = <2>;

+        /* EIM_CSnGCR1, EIM_CSnGCR2, EIM_CSnRCR1, EIM_CSnRCR2, EIM_CSnWCR1, EIM_CSnWCR2 */

+        fsl,weim-cs-timing = <0x40B184B1 0x00001010 0x14017000

+                0x00000000 0x14000E00 0x00000000>;

+    };

+};

Hope it helps!

0 件の賞賛
返信

4,331件の閲覧回数
durmus
Contributor IV

Thank you for your quick reply.

We are planning to use 23LCV1024 SPI SRAM from Microchip. I couldn't find a specific driver for it so I'm looking for something to start with.

I had thought maybe you were using something similar, rather than a flash memory. But thanks anyway, it will be very helpful.

0 件の賞賛
返信

4,331件の閲覧回数
_andev_
Contributor II

Hi all,

Finally the solution come from changing the values of 'fsl,weim-cs-timing'. All the other things are ok.

Regards

0 件の賞賛
返信

4,331件の閲覧回数
Poussemousse
Contributor III

Hello,

I have also some trouble with my external SRAM, could you please give your corrected timing fsl,weim-cs-timing configuration ?

I am able to have correct individual access, but as soon as I try to get fast consecutive access, I have a big dead time of around 380ns between two readings, and 360ns between two writings.

Thanks a lot.

0 件の賞賛
返信

4,331件の閲覧回数
_andev_
Contributor II

Hi Poussemousse,

Sorry for the delay! We're facing similar issues. We have right consecutive reads but consecutives writes we can

see long delays like you. Our weim and sram configuration is:

&weim {

    pinctrl-names = "default";

    pinctrl-0 = <&pinctrl_weim_ram_1 &pinctrl_weim_cs0_1>;

    #address-cells = <2>;

    #size-cells = <1>;

    /* <cs-number> 0 <physical address of mapping> <size> = size 64MB -> addr=22 pins*/

    ranges = <0 0 0x08000000 0x008000000>;

    status = "okay";

    sram@0,0 {

        compatible = "mtd-ram";

        reg = <0 0 0x00400000>;

        #address-cells = <1>;

        #size-cells = <1>;

        bank-width = <2>;

        /* EIM_CSnGCR1, EIM_CSnGCR2, EIM_CSnRCR1, EIM_CSnRCR2, EIM_CSnWCR1, EIM_CSnWCR2 */

        fsl,weim-cs-timing = <0x00010CB1 0x00001010 0x0C015100

                0x00000000 0xCC1C7640 0x00000000>;

    };

};

It seems that the writing delay match the weim watchdog time. Once the watchdog is fired the write is done.

Have you solve the issue??

Regards

0 件の賞賛
返信

4,331件の閲覧回数
Poussemousse
Contributor III

Hi,

Thank you for your feedback, unfortunately it doesn't solve our problem.

Using iMX6S, we are interfacing a 16bits parallel 45ns asynchronous SRAM, and the only way to have consecutive accesses without dead time is to widen the bus.

EIM bus registers :

EIM_CS1GCR1 00010001

EIM_CS1GCR2 00000000

EIM_CS1RCR1 03000000

EIM_CS1RCR2 00000008

EIM_CS1WCR1 03000000

EIM_CS1WCR2 00000000

I explain :

With a 16 bits configuration : reading or Writing 2 different words of 16 bits, imply to wait for about 250/280ns between the 2 accesses.

In the following pictures, we observe CS signal.

With a 32 bits configuration : reading 2 different words of 16 bits, through 2 consecutive accesses doesn't any dead time (90ns time  = 2 very consecutive access of our 45ns SRAM)  , but than we have to wait again for about 270ns between the 2 words of 32 bits.

S4GMENU_Uboot_lecture_SRAM.png

With a 64 bits configuration: writing 1 words of 64bits = 4x 16bits word, through 4 consecutive accesses doesn't any dead time (180ns = 4x45ns) , but then we have to wait again for about 332ns for next 64 bits word Write

S4GMENU_Uboot_ecriture_SRAM.png

We are wondering if it is due to internal bus Exchange into the iMx6 which could explain this pain.

Any help would be very appreciated.

Poussemousse

0 件の賞賛
返信

4,331件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please refer to chapter "EIM NOR Driver" of "i.MX_6_Linux_Reference_Manual.pdf".

In particular :

"Similar to the SPI NOR, the parallel NOR uses the MTD subsystem. Because the parallel
NOR is very small, you may only use the jffs2 but cannot use the UBIFS for it."

and

"Add weim-nor to the kernel command line to enable the WEIM NOR. The WEIM NOR

has pin conflict with some other modules, such as the SPI."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信