SPSDK support for i.MXRT116X platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPSDK support for i.MXRT116X platform

353 Views
vishnusudhankj
Contributor III

Hi,

I have read the SPSDK document and the usages of its API commands.

I have a few questions, which I'll address below:

1. For i.MXRT1160, listed like i.Mx RT 1170 / 1160(blhost) in support devices

Does that imply support for the BLHOST command alone on the i.mxrt 116x series board?

2. I am unable to view board option 116x in the nxpimage command. Does the i.mxrt 116x board have the option?

3. Does the SPSDK support the i.MXRT116x series boards with its accessible commands? because I can't see the board choices as rt116x in the majority of commands.

 

 

Tags (1)
0 Kudos
Reply
1 Reply

333 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

1- No, RT11xx has support for other tools besides blhost. BLHost is the tool to communicate with the ROM bootloader of the RT devices:

Omar_Anguiano_0-1670356942028.png

2- Unfortunately, there is no specific option.

3- Yes, it is likely that RT1160 is supported by RT1170 commands.

Best regards,
Omar

0 Kudos
Reply