SPSDK support for i.MXRT116X platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPSDK support for i.MXRT116X platform

360件の閲覧回数
vishnusudhankj
Contributor III

Hi,

I have read the SPSDK document and the usages of its API commands.

I have a few questions, which I'll address below:

1. For i.MXRT1160, listed like i.Mx RT 1170 / 1160(blhost) in support devices

Does that imply support for the BLHOST command alone on the i.mxrt 116x series board?

2. I am unable to view board option 116x in the nxpimage command. Does the i.mxrt 116x board have the option?

3. Does the SPSDK support the i.MXRT116x series boards with its accessible commands? because I can't see the board choices as rt116x in the majority of commands.

 

 

タグ(1)
0 件の賞賛
返信
1 返信

340件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

1- No, RT11xx has support for other tools besides blhost. BLHost is the tool to communicate with the ROM bootloader of the RT devices:

Omar_Anguiano_0-1670356942028.png

2- Unfortunately, there is no specific option.

3- Yes, it is likely that RT1160 is supported by RT1170 commands.

Best regards,
Omar

0 件の賞賛
返信