SPI without MISO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPI without MISO

跳至解决方案
1,858 次查看
mustafademirci
Contributor I

Instead of building an SPI port with MOSI and MISO lanes, is it possible to have two symmetric seperate SPI interface with only MOSI lanes between i.MX6 and an FPGA?

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,621 次查看
igorpadykov
NXP Employee
NXP Employee

HI Mustafa

seems one can use configuration with

one interface as master, other slave.  One can look at

IMX6DQRM  sect.21.1.2 Modes and Operations

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,622 次查看
igorpadykov
NXP Employee
NXP Employee

HI Mustafa

seems one can use configuration with

one interface as master, other slave.  One can look at

IMX6DQRM  sect.21.1.2 Modes and Operations

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复