I am struggling with an spi issue on imx6ul.
Any pointer will be helpful to fix / debug this issue
When I trace the SPI line, it seems that there us a drift in CS line, Also on clk line there are sometime 7 pulses and sometime 8 pulses.
Below is my device tree setting
spi0 = &ecspi2;
&ecspi2 { 
 pinctrl-names = "default"; 
 pinctrl-0 = <&pinctrl_ecspi2>; 
 fsl,spi-num-chipselects = <1>; 
 cs-gpios = <&gpio1 10 1>; 
 status = "okay";
 spidev0: spi@0 { 
    compatible = "spidev"; 
    reg = <0>; 
    spi-max-frequency = <10000000>; 
    }; 
};
pinctrl_ecspi2: ecspi2grp { 
 fsl,pins = < 
 MX6UL_PAD_JTAG_MOD__GPIO1_IO10 0x0b0b0 /* CSPI_SS */ 
 MX6UL_PAD_UART5_TX_DATA__ECSPI2_MOSI 0x0b0b0 /* CSPI_MOSI */ 
 MX6UL_PAD_UART5_RX_DATA__ECSPI2_MISO 0x0b0b0 /* CSPI_MISO */ 
 MX6UL_PAD_UART4_TX_DATA__ECSPI2_SCLK 0x0b0b0 /* CSPI_SCLK */ 
 >; 
};
 
					
				
		
There was a bug in the i.MX53 clock setup that stopped the SPI clocks and the SPI sending when the CPU "slept". it is unlikely that this problem is in the far newer kernel that you're using, but it may have crept in.
https://community.nxp.com/message/593611#comment-587236
There were all sorts of other bad problems with the CURRENT i.MX53 SPI Linux Drivers that made them useless for us, but they were fixed in 2.6.38 as the drivers were replaced by the "mainline" ones. You distribution should have the newer one. Details here:
https://community.nxp.com/message/593611#comment-585209
Tom
Thanks Tom for your reply.
The thread you posted had mentioned 2.6.35 kernel and for the imx53 & imx28.
Here I am using 4.4. kernel and imx6ul, is it same issue been discussed in these threads ?
With Regards
Anand
 
					
				
		
You should search for "eCSPI" in the Search Box. There are a lot of previous issues there. Some may relate to your problem. One is having a problem with chip-selects, partly because the driver supports them as very slow GPIOs which the software turns on and off, rather than having the better solution where the hardware CS lines are used instead.
i.MX53 is only supported by Freescale with 2.6.35. The SPI drivers were quite buggy.
2.6.38 was released for some reason, but isn't the "official" release for i.MX53.
The Freescale SPI drivers in 2.6.35 were replaced with "mainline" drivers in 2.6.38.
I would assume (but don't know) that the "mainline" drivers were used in 3.x and 4.x Linux.
The Link in my post (above) links to the post detailing one of the problems I had with SPI. Those problems weren't in the SPI driver itself, but in the "platform setup" code that controlled the master clock power modes. As detailed in my post, in 2.6.35 this was set in "arch/arm/mach-mx5/system.c". I have no idea how this is set up in 4.4 and on the i.MX6 (this stuff tends to move around), but suggest you check the i.MX53 and i.MX6 Reference Manuals, find the equivalent control registers and search for any code in 4.4 doing the same thing.
This is unlikely to be related to your problem.
> there us a drift in CS line
What do you mean by that? "Drifting" in level up and down or time early and late? You can expect a lot of variation in time as they're being driven as GPIOs in software. In this post there's a clock glitch, and sometimes I think it said the chip-select was too late and happened after the eCSPI had started clocking:
https://community.nxp.com/thread/386935#comment-625531
The "7 or 8 pulses" is just plain weird. something seriously wrong there.
Tom
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Anand
one can check ECSPIx_CONREG[BURST_LENGTH] value described in
sect.20.7.3 Control Register (ECSPIx_CONREG) i.MX6UL Reference Manual
and that during transmitting burst fifo was not empty.
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks igor for your reply
Just wanted to know before trying that, is the vaule of ECSPIx_CONREG[BURST_LENGTH] is related to the clock issue ?
Regards
Anand