SPI interface with IMX6 solo processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI interface with IMX6 solo processor

1,725 次查看
subhashreechand
Contributor I

Hello All,

I want to interface MCP2515 (CAN Controller) with IMX6 solo processor via SPI .

what is the procedure to do this?

Can anyone help me on this ?

0 项奖励
回复
3 回复数

1,511 次查看
mtx512
Contributor V

The i.mx6 SoloX has a built in CAN controller (Flexcan) so using the MCP2515 is overkill. You can use a CAN transceiver eg SN65HVD232 with Flexcan.

0 项奖励
回复

1,511 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,511 次查看
subhashreechand
Contributor I

Hello Joan Xie ,

Thanks for the reply .

But that post speaks about the Kernel version.

I am trying to write the  code , build it and copy the bin  to the SD card and then flash the bin to the processor.

My question : what are the steps to code to make the MCP2515 transmit/receive a CAN signal to the i.MX6 SoloX processor ?

0 项奖励
回复