SPI driver Sabre lite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPI driver Sabre lite

跳至解决方案
2,049 次查看
niklasmolin
Senior Contributor I

Hi.

I'm trying the nitrogen6x build for the Sabre lite board and trying to enable the SPIdev driver (In Yocto).

I have changed the alias in the board-mx6_nitrogen6x.c file and also updated the defconfig (I think it's the right one) to enable SPIDEV etc.

But I still don't see spidev under /dev directory.

Is there anything else I'm missing here?

I managed to get it work when I was using sabrelite as "MACHINE", for about 2 months ago.

Thanks,

Niklas

标签 (2)
0 项奖励
回复
1 解答
1,290 次查看
EricNelson
Senior Contributor II

Hi Niklas,

The default kernel configuration has support for SPI. You can validate this by looking in /proc/mtd to see the flash partitions and you can run "hexdump -c /dev/mtd0r0" to see the content of SPI-NOR.

It seems that you're asking about userspace SPI access though (/dev/spi...). This isn't included in the standard kernel configuration, and you'd need to enable it by running "bitbake -c menuconfig linux-boundary".

I wonder why you're doing this though. Are you hooking up a different SPI device through other pins? If so, you'll need to change the pin-muxing for the SPI and chip-select pins and add another SPI bus to the system as shown here:

     linux-imx6/arch/arm/mach-mx6/board-mx6_nitrogen6x.c at boundary-imx_3.0.35_4.1.0 · boundarydevices/l...

If you're doing this level of kernel hacking, I'd strongly recommend building the kernel outside of Yocto, so that you have a proper git repository backing your efforts.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,291 次查看
EricNelson
Senior Contributor II

Hi Niklas,

The default kernel configuration has support for SPI. You can validate this by looking in /proc/mtd to see the flash partitions and you can run "hexdump -c /dev/mtd0r0" to see the content of SPI-NOR.

It seems that you're asking about userspace SPI access though (/dev/spi...). This isn't included in the standard kernel configuration, and you'd need to enable it by running "bitbake -c menuconfig linux-boundary".

I wonder why you're doing this though. Are you hooking up a different SPI device through other pins? If so, you'll need to change the pin-muxing for the SPI and chip-select pins and add another SPI bus to the system as shown here:

     linux-imx6/arch/arm/mach-mx6/board-mx6_nitrogen6x.c at boundary-imx_3.0.35_4.1.0 · boundarydevices/l...

If you're doing this level of kernel hacking, I'd strongly recommend building the kernel outside of Yocto, so that you have a proper git repository backing your efforts.

0 项奖励
回复
1,290 次查看
niklasmolin
Senior Contributor I

Hi Eric.

Thanks for you reply.

This was definitely helpful, since we just wanted to access the flash to do some tests.

Thanks,

Niklas

0 项奖励
回复