SPI-NOR boot in i.MX53 ARD board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI-NOR boot in i.MX53 ARD board

Jump to solution
1,327 Views
ko-hey
Senior Contributor II

Hi all

I have a problem in NOR boot of my customer original board with i.MX53 so try to test with i.MX53 ARD board for comparison.

However, we couldn't boot from serial NOR.

Please tell me how to NOR boot in i.MX53 ARD board.

My trial steps are as below.

---------------------------------

1. Boot from SD.

2. Tried initialization of SPI-NOR by reference to chapter 3.5 of uboot_mx5x.pdf.

3. Got error message as follows after using "sf probe" command.

MX53-ARD-DDR3 MFG U-Boot > sf probe 1

JEDEC ID: 0x20:0x20:0x16

Failed to initialize SPI flash at 0:1

MX53-ARD-DDR3 MFG U-Boot >

---------------------------------

What shuold I do for it ?

Fothermore, if someone have a successful experience to boot from SPI-NOR in i.MX53 ARD board, please share the ucl.xml file.

Ko-hey

Labels (2)
0 Kudos
1 Solution
1,022 Views
jimmychan
NXP TechSupport
NXP TechSupport

I think the board is able to boot from NOR flash. But the BSP is not supported due to the pin conflict with Ethernet (using the same EIM pins).

View solution in original post

0 Kudos
4 Replies
1,022 Views
jimmychan
NXP TechSupport
NXP TechSupport

According to the release note, the SPI-NOR is not supported on i.MX53 ARD board due to the pin conflict with Ethernet.

0 Kudos
1,022 Views
ko-hey
Senior Contributor II

So why it mentioned in Quick Start Guide ?

Please see P8 of the attachment.

0 Kudos
1,023 Views
jimmychan
NXP TechSupport
NXP TechSupport

I think the board is able to boot from NOR flash. But the BSP is not supported due to the pin conflict with Ethernet (using the same EIM pins).

0 Kudos
1,022 Views
ko-hey
Senior Contributor II

I understand. Thank you.

Ko-hey

0 Kudos