Hi All,
We are planning to use Micron's SPI NAND chip(MT29F4G01) in i.mx6q SOC based custom hardware. We have got spi nand driver from microns, Let me know how to integrate these driver in i.mx6 linux 4.1.15 BSP. In the Linux BSP we have seen only i.mx6 SPI nor controller driver. Will it work for a SPI NAND flash driver? or how do we port the driver in 4.1.5 to make it detect.
Thanks in Advance,
Shabeer
Hi Shabeer
one can try to follow micron porting documentation
Micron TN-00-25: Enabling a Flash Memory Device into the Linux MTD
https://www.micron.com/~/media/documents/products/technical-note/nand-flash/tn0025_enabling_flash_in...
[v2,5/6] nand: spi: add Micron spi nand support - Patchwork
use as example NXP spi-nor driver described in attached Linux Manual
Chapter 31 SPI NOR Flash Memory Technology Device (MTD) Driver
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
Thanks for the quick response.
Do we need to do modifiy the imx6 spi-nor controller driver for adapting this flash chip?
Best Regards,
Shabeer