current I use IMX6ULL, I meat a SPI DMA issue.
I configated SPI as POL=0, PHA=1. When I use SPI polling to do data transfer, then it is OK.
But when I use SPI DMA to do data transfer, then the SPI timing look like POL=0, PHA=0.
what is wrong with it? is there something wrong configuration while in SPI DMA or in SPI DMA, IMX6ULL only support POL=0, PHA=0?
Hi liqi
what bsp used in the case, please try nxp official bsp from
source.codeaurora.org/external/imx/linux-imx repository
Documentation
i.MX Software and Development Tools | NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi <https://community.nxp.com/people/igorpadykov?et=watches.email.thread> igorpadykov,
Just as you said, I try it on the IMX6ULL EVK. But the result is same as I said in previously email. The timing is attached.
Have you also try it?
//SPI configuration: baudRate_Bps=20000000 burstLength = 32
static void ECSPI_GetDefaultChannelConfig(ecspi_channel_config_t *config)
{
config->channelMode = kECSPI_Slave; /!< ECSPI peripheral operates in slave mode./
config->clockInactiveState = kECSPI_ClockInactiveStateLow; /*!< Clock line (SCLK) inactive state */
config->dataLineInactiveState = kECSPI_DataLineInactiveStateLow; /*!< Data line (MOSI&MISO) inactive state */
config->chipSlectActiveState = kECSPI_ChipSelectActiveStateLow; /*!< Chip select(SS) line active state */
config->waveForm = kECSPI_WaveFormSingle; /*!< ECSPI SS wave form */
config->polarity = kECSPI_PolarityActiveHigh; /*!< Clock polarity */
config->phase = kECSPI_ClockPhaseSecondEdge; /*!< clock phase */
}
Thanks!
wuliqi
发件人: bounces+210748-fda0-liqi_wu=163.com@jiveon.jivesoftware.com 代表 igorpadykov
发送时间: 2020年1月14日 14:39
收件人: liqi wu <liqi_wu@163.com>
主题: Re: - Re: SPI DMA issue for IXM6ULL
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community
Re: SPI DMA issue for IXM6ULL
reply from igorpadykov <https://community.nxp.com/people/igorpadykov?et=watches.email.thread> in i.MX Processors - View the full discussion <https://community.nxp.com/message/1254956?commentID=1254956&et=watches.email.thread#comment-1254956>
Hi igorpadykov,
I will try it on IMX6ULL EVK board.
I hope you also can try it if possible.
发件人: bounces+210748-fda0-liqi_wu=163.com@jiveon.jivesoftware.com 代表 igorpadykov
发送时间: 2020年1月14日 14:39
收件人: liqi wu <liqi_wu@163.com>
主题: Re: - Re: SPI DMA issue for IXM6ULL
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community
Re: SPI DMA issue for IXM6ULL
reply from igorpadykov <https://community.nxp.com/people/igorpadykov?et=watches.email.thread> in i.MX Processors - View the full discussion <https://community.nxp.com/message/1254956?commentID=1254956&et=watches.email.thread#comment-1254956>