SPI Burst Transfer in linux imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Burst Transfer in linux imx6

4,739件の閲覧回数
kunalkotecha
Contributor II

Hello all,

I am using imx6ull on a custom board with linux 4.1.15 and currently working on SPI peripheral. I am using IMX6ULL as a Master and DTS for the same is as below :

&ecspi2 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi2>;
fsl,spi-num-chipselects = <1>;
cs-gpios = <&gpio1 29 0>;
   spidev1: spi@1 {
      reg = <0>;
      compatible = "spidev";
      spi-max-frequency = <250000>;
      status = "okay";
   };

};

We used spidev.c as driver for interfacing and did 1 change in it as below:

static const struct of_device_id spidev_dt_ids[] = {
      { .compatible = "rohm,dh2228fv" },
      { .compatible = "spidev" },
      {},
};
and found the device node as /dev/spidev1.0.

It is working properly and able to see pulses of all the pins properly. But We want to transfer more than 1 byte at a time. So in Burst transfer, we are not getting continuous clock pulse and chip select. Hence, at every byte, CS deactivates and then activates again. I tried by cs_change = 0, but still facing issue. Please help me out of it to disable toggling of CS at every byte transfer? 

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

3,134件の閲覧回数

Hi, Igor

I applied patch to 4.9.11 kernel and have a problems.

I want to make multiple (from 2  up to 17) bytes burst transfer (tx and rx) but spi output is broken. Data are broken on any transfer with size > 4 and size!=(4*n) in bytes.

When I send 1,2,3,4 in one burst - it ok

When I send 1,2,3,4,5 in one burst - i see 4,0,0,0,5 on SPI output with logic analyzer

When I send 1,2,3,4,5,6 in one burst - i see 3,4,0,0,5,6 on SPI output with logic analyzer

0 件の賞賛
返信

3,134件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kunal

please try patch on

spi-imx: imx6q add single burst transfer support - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信