Hello everyone,
I am planning to use an i.MX 8M Plus SOM to display images on a 1920x720 display with 2 LVDS displays:
My question is do I need to use both of the SOM LVDS interfaces (in split mode) ? if that's the case do I need to use one LVDS port for odd pixels/pins and the other for the even pixels/pins ?
Also any bsp or design example is more than welcome.
Thank you!
BTW: Here you may find a dual-channel example albeit using a bridge rather than a display.
This looks like a regular dual-channel LVDS display which should be supported. However, a more interesting aspect of such displays is their pixel mapping which should also be mentioned in the Datasheet (BTW: What exact display make/model is it?). That said there are more or less only two possibilities called JEIDA or VESA and both should be supported.
On this topic, I have an additional question: Table 13-33. Pixel Mapper Modes of the i.MX 8M Plus Applications Processor Reference Manual, Rev. 1, 06/2021 mentions both Dual and Split mode but does not further explain anything about it. What exactly are those?
My understanding is, that the i.MX 8M Plus only supports one single LVDS display. Is that a correct assumption or can two (albeit single-channel only) displays be connected concurrently?
Hi NXP,
We are also facing the same question on i.mx8mp. It is no problems to support one single channel or one dual-channel lvds display. Could the lvds interface support two single channel lvds display and how?
-Eric
I don't think it is true. i.MX8M Plus can only supports one single-channel or one dual-channel LVDS interface because there is only one lcdif2 controllers. Unlike i.MX6, there are two IPU controllers that can support two separate LVDS displays. If i.MX8M Plus can support two single separate LVDS displays, how do you make device tree to work?
-Eric