[SOLVED] imx28_LTIB_Problems with keyboard

cancel
Showing results for 
Search instead for 
Did you mean: 

[SOLVED] imx28_LTIB_Problems with keyboard

219 Views
Nico
Contributor II

This is the message that i see when the filesystem is loaded

 

(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base

(EE) XKB: No components provided for device Virtual core keyboardunrecognised device identifier!

(EE) config/hal: NewInputDeviceRequest failed (2)unrecognised device identifier!

(EE) config/hal: NewInputDeviceRequest failed (2)unrecognised device identifier!

(EE) config/hal: NewInputDeviceRequest failed (2)

matchbox: keyboard does not appear to have a <alt> key.

matchbox: ignoring key shortcut <Alt>n=next

 

The message is the same also without the keyboard attached...

 

Is it a problem of matchbox? How can i solve this problem?

Thanks in advance!!

Labels (1)
0 Kudos
1 Reply

42 Views
Nico
Contributor II
Thanks to Danny Chin for startx file. It's just necessary copy the attached file in ..ltib/rootfs/usr/bin/ and it works!!
0 Kudos