SNVS in non-secure state

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SNVS in non-secure state

1,808 次查看
kevi49
Contributor II

I have enabled the SNVS in kernel

And I am checking the log in dmesg and it is showing that 

"caam-snvs 20cc000.caam-snvs: violation handlers armed - non-secure state"

 

So, how to secure it?

What steps I need to follow?

标记 (3)
0 项奖励
回复
2 回复数

1,790 次查看
kevi49
Contributor II

Hi @Bio_TICFSL ,

 

Thank you for answer.

 

I have one query regarding the tamper detection in LP mode.

#define SNVS_HPSICR 0xc
        #define SNVS_HPSICR_VALUE 0x80000035

#define SNVS_LPTGFCR 0x44
        #define SNVS_LPTGFCR_VALUE 0x800000

#define SNVS_LPTDCR 0x48
        #define SNVS_LPTDCR_VALUE 0xa00

#define SNVS_LPZMK 0x6c
        #define SNVS_LPZMK_VALUE 0x12345678

#define SNVS_LPSR 0x4c
        #define SNVS_LPSR_RESET_VALUE 0x7f0

#define SNVS_TAMPER 0xa4
        #define SNVS_TAMPER_RESET_VALUE 0xff

 

Step 1: Configured all above register.

Step 2: Disconnected the main power supply, and device is now operating in LP mode with coin cell.

Step 3: Press the tamper switch.

Step 4: Again turn the board on with main power source(HP Mode).

Step 5: Reading the register SNVS_LPSR(4c) value to check if tamper bit 9(ET1D) if set or not.

Step 6: But it showing always 0, even after tamper switch is press.

All above configuration working properly in HP mode(After pressing switch if I read the SNVS_LPSR(4c) it showing tamper bit 9(ET1D) is set).

 

So, what is the wrong here,Why I am not able to see the bit is set in LP mode(After removing main power source).

 

 

0 项奖励
回复

1,801 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Please refer to section 6.3.1.1 (Transitioning among system security monitor states)

of the i.MX6 Security Reference Manual.

 

https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLSRM&appType=moderatedWithoutFAE&fasp=1&WT_TYPE... 

Regards

Have a great day,

0 项奖励
回复