SNVS Regulator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SNVS Regulator

1,818 Views
eishishibusawa
Contributor III

Dear Sir

 

I refer to the IMX6SDLRM Rev.4.

P4516 51.5 SNVS Regulator

If VDDHIGH_IN is present, then the SNVS_IN supply is internally shorted to the VDDHIGH_IN supply.

VDDHIGH_IN can be separated from SNVS_IN by setting the PMU_MISC0[discon_high_snvs] bit.

 

P910 CCM_ANALOG_MISC0n field descriptions (continued)

discon_high_snvs : This bit forces the short between VDDHIGH_IN and VSNVS_IN to open when asserted. This is useful in power cases where SNVS_IN > VDDHIGH_IN.

 

I refer to the schematic of MCIMX6DL-SDP (SPF-27417_C5.pdf).

VDDHIGH_IN_1/2 = VDDHIGH_IN = VGEN5 = 2.8V

VDD_SNVS_IN = VSNVS_3V0 = 3.0V

(SNVS_IN > VDDHIGH_IN)

 

Q1.

Is it necessary to set PMU_MISC0[discon_high_snvs] bit when designing like MCIMX6DL-SDP?

 

Best Regards,

Eishi SHIBUSAWA

Labels (2)
0 Kudos
Reply
1 Reply

1,326 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

your understanding is correct and more described in Table 2-6. Power and decouple

recommendations i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

This setting may be useful in battery powered designs.

However in case MCIMX6DL-SDP design SNVS_IN is powered from

pmic PMIC_VSNVS and its SNVS current provided from VIN which eventually is

powered from board external 5V/5A universal DC power supply, not from LICELL so

coincell will not be discharged to VDDHIGH_IN. Pmic VSNVS generation is described in

sect.6.4.7VSNVS LDO/Switch  MMPF0100 Datasheet

https://www.nxp.com/docs/en/data-sheet/MMPF0100.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply