SN65DSI86 bridge connection issue with MIPI_DSI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SN65DSI86 bridge connection issue with MIPI_DSI

267件の閲覧回数
Cyriactoms
Contributor III

Mipi dsi not able to attach the sn65dsi bridge. The driver is loading fine but it gives an error like this   [ 7.223851] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/bus@32c00000/mipi_dsi@32e60000 to encoder DSI-40: -19
[ 7.240955] imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to attach bridge: 32e60000.mipi_dsi
[ 7.249236] DSIM_DEBUG: sec_mipi_dsim_bind() returned -19
[ 7.261771] imx_sec_dsim_drv 32e60000.mipi_dsi: failed to bind sec dsim bridge: -19
[ 7.269436] imx-drm display-subsystem: bound 32e60000.mipi_dsi (ops imx_sec_dsim_ops)

 

vcc_1v2: regulator-vcc-1v2 {
compatible = "regulator-fixed";
regulator-name = "vcc_1v2";
regulator-min-microvolt = <1200000>;
regulator-max-microvolt = <1200000>;
regulator-always-on;
regulator-boot-on;
};

vcc_1v8: regulator-vcc-1v8 {
compatible = "regulator-fixed";
regulator-name = "vcc_1v8";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
regulator-boot-on;
};

panel_edp: panel {
compatible = "lg,lp079qx1-sp0v";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_mipi_dsi_en>;
status = "okay";

port {
panel_in: endpoint {
remote-endpoint = <&edp_bridge_out>;
};
};

display-timings {
native-mode = <&timing_1280x800>;

timing_1280x800: 1280x800 {
clock-frequency = <77000000>; /* 77.00 MHz */
hactive = <1280>;
vactive = <800>;

hfront-porch = <160>;
hsync-len = <32>;
hback-porch = <40>; /* Calculated: 232 - 160 - 32 */

vfront-porch = <20>;
vsync-len = <6>;
vback-porch = <30>; /* Calculated: 56 - 20 - 6 */
};
};

};

refclk: input_refclk{
compatible = "fixed-clock";
#clock-cells = <0>;
clock-frequency = <19200000>;
clock-output-names = "refclk";
};
};
 
&lcdif1 {
status = "okay";
lcdif1_disp: port@0 {
reg = <0>;

lcdif_to_dsim_1: endpoint {
remote-endpoint = <&dsim_from_lcdif_2>;
};
};
};

&mipi_dsi {
status = "okay";

ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
dsim_from_lcdif_2: endpoint {
remote-endpoint = <&lcdif_to_dsim_1>;
};
};
port@1 {
reg = <1>;
dsim_to_edpbridge: endpoint {
remote-endpoint = <&edp_bridge_in>;
};
};
};
};


&i2c3{
clock-frequency = <400000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c3>;
status = "okay";
 
 
sn65dsi86_bridge: sn65dsi86@2c{
compatible = "ti,sn65dsi86";
reg = <0x2c>;
status ="okay";

pinctrl-names = "default";
pinctrl-0 = <&pinctrl_dp>;

enable-gpios = <&gpio1 5 GPIO_ACTIVE_HIGH>;

vccio-supply = <&vcc_1v8>;
vpll-supply = <&vcc_1v8>;
vcca-supply = <&vcc_1v2>;
vcc-supply = <&vcc_1v2>;

clock-names = "refclk";
clocks = <&refclk>;


ports{
#address-cells = <1>;
#size-cells = <0>;
 
port@0 {
reg = <0>;

edp_bridge_in: endpoint {
remote-endpoint = <&dsim_to_edpbridge>;
data-lanes = <0 1 2 3>;
};
};
port@1 {
reg = <1>;

edp_bridge_out: endpoint {
remote-endpoint = <&panel_in>;
data-lanes = <0 1 2 3>;
};
};
 
};
};
 
 
Does it work with i2c when i tried i2cdump its giving xx values for every register and also
 
cat /sys/kernel/debug/regmap/2-002c/registers giving xx values is this the cause for the mipi dsi to bind
 
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

209件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

What the regulator do? if marked the fails on regulator but I can not tested since we have no SN65DSI at hand, you should try to change this.

Regards

0 件の賞賛
返信