Hi Jing
Thank you for the reply.
Maybe you can assist me with getting my custom board to program?
This board just came from assembly house ans SWD programming does not work. I see the Clock pulses on SWD_CLK and on SWD_DIO pins. 3.3V available on VCC and nRST does respond.
Error output from MCUXpresso Jlink interface below. I am currently using a J-Link Edu Mini. Should I use some other tool?
Error
ERROR: Could not connect to target.
SEGGER J-Link GDB Server V7.86e Command Line Version
JLinkARM.dll V7.86e (DLL compiled Mar 22 2023 16:27:41)
Command line: -SettingsFile C:\Projects\NXP Dev Kits\Alexa_Dev_kit-software\sln_alexa_iot_iled_blinky\Debug\sln_alexa_iot_iled_blinky JLink Debug SettingsFile.jlink -nosilent -swoport 2332 -select USB -telnetport 2333 -endian big -noir -speed 4000 -port 2331 -vd -device MIMXRT106SDVL6A -if SWD -halt -reportuseraction
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: off
Silent mode: off
Single run mode: off
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: C:\Projects\NXP Dev Kits\Alexa_Dev_kit-software\sln_alexa_iot_iled_blinky\Debug\sln_alexa_iot_iled_blinky JLink Debug SettingsFile.jlink
------Target related settings------
Target device: MIMXRT106SDVL6A
Target device parameters: none
Target interface: SWD
Target interface speed: 4000kHz
Target endian: big
Connecting to J-Link...
J-Link is connected.
Device "MIMXRT106SDVL6A" selected.
Firmware: J-Link EDU Mini V1 compiled Mar 15 2023 11:22:34
Hardware: V1.00
S/N: 801037084
Feature(s): FlashBP, GDB
Checking target voltage...
Target voltage: 3.13 V
Listening on TCP/IP port 2331
Connecting to target...
InitTarget() start
InitTarget() end - Took 102ms
$$UserActionStart$$: Terms of use
$$UserActionEnd$$: Terms of use
Failed to attach to CPU. Trying connect under reset.
InitTarget() start
InitTarget() end - Took 105ms
ERROR: Could not connect to target.