SGTL5000 CPFILT in battery powered applications

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGTL5000 CPFILT in battery powered applications

796件の閲覧回数
jonpry
Contributor I

Regarding the SGTL5000 datasheet, on page 4, Table 1, it lists that the CPFILT must be installed if VDDIO and VDDA are both < 3.0V, otherwise it must not be installed.

In my application one of both of these supplies will be battery powered with a range of 2.0 - 3.3 volts. Is this configuration not possible because of the charge pump?

0 件の賞賛
返信
1 返信

739件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jonathan

if one of these voltages >3.0 V, the CPFILT cap must not be placed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信