SEMC SRAM interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SEMC SRAM interface

2,420 次查看
ShiXiang
Contributor I

product: I.mxrt 1170 series

For the SRAM write/read in SYNC mode (ADMUX), just wonder is it possible to mask the higher address bit, A[M : 16], means not to use and free up my address pin, so that I can connect them extra GPIOs.

My SRAM application only need A0-15. 

SEMC SRAM masking.jpg

0 项奖励
回复
3 回复数

2,386 次查看
art
NXP Employee
NXP Employee

Yes, it is possible to use upper address pins (A16 and higher) as GPIOs when
SEMC operates in SRAM mode. Just configure these pins as GPIOs in IOMUXC.

Best Regards,
Artur

0 项奖励
回复

2,396 次查看
ShiXiang
Contributor I

No reply yet, re-post to I.MX RT page.

Please close this question, thank you. 

 

 

 

0 项奖励
回复

2,413 次查看
ShiXiang
Contributor I

Can the software call function/register support on masking or is the software/register adjustable? For masking the higher address bit, A[M : 16], while using SRAM write/read in SYNC mode (ADMUX) . Thank you. 

0 项奖励
回复