SELinux support for SABRE auto BSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SELinux support for SABRE auto BSP

1,709 次查看
vishakh
Contributor III

Hi,

I am trying to include SElinux in sabreauto BSP (NXP Yocto release imx-3.10.53-1.1.0_ga).

As I am new to Yocto I need some suggestion to do this.

This is what I have done so for:

  • Cloned the meta-selinux from git://git.yoctoproject.org/meta-selinux
  • Included meta-selinux path to imx6qsabreauto/conf/bblayers.conf
  • Have set the DISTRO="poky-selinux"  in imx6qsabreauto/conf/local.conf
  • Built the image using "bitbake fsl-image-gui".

Here I am getting "No recipes available message".

Seems like I have missed many things here. Any suggestions will be helpful.

With Regards,

Vishakh

0 项奖励
回复
1 回复

1,280 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vishakh

please refer to

meta-selinux - Layer enabling SELinux support. 

Yocto Training - home 

https://community.freescale.com/docs/DOC-95333

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复