SDcard booting issues on IMX8MPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDcard booting issues on IMX8MPlus

Jump to solution
754 Views
Saravanans1
Contributor III

Hi,

We have an IMX8MPlus custom board unable to boot after u-boot. Below is the SD image generated in our build with a size of 260 MB.

imx8mplus-image-auaq0010-mna00012-7in-usd.wic.zst

After this, I flashed this image to a 32GB Sandisk SD card using the below command

zstdcat imx8mplus-image-auaq0010-mna00012-7in-usd.wic.zst | sudo dd of=/dev/sdX bs=1M conv=fsync

Note:
1. Format the SD card to "FAT32" before flashing the actual SD image.
2. Replaced the sdX as "sde" with the one which was detected by our host machine for uSD.

Then we inserted this flashed SD card to our board and tried to boot using SD mode.

However, we are unable to boot from the SD card and observed below-mentioned errors from the console. Please refer to the attached boot log for more details.

Failed to load 'boot.scr'
Error reading cluster
** Unable to read file Image **
Failed to load 'Image'
END BOOTING
u-boot=>

u-boot=> mmc part
Partition Map for MMC device 1 -- Partition Type: DOS
Part Start Sector Num Sectors UUID Type
** Can't read partition table on 1:0 **
u-boot=>

Please provide any other methods/suggestions such as any particular Filesystem Type needs to be considered while flashing the SD card, so that it is easy for me to fix this issue.

0 Kudos
Reply
1 Solution
736 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please try bmaptool to flash wic image.

IMAGE=fsl-image-multimedia-full-imx8mqevk-20181018224131.rootfs.wic
DEVICE=/dev/sdb # The device may change in your system
sudo bmaptool copy $IMAGE $DEVICE --nobmap

 

View solution in original post

0 Kudos
Reply
1 Reply
737 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please try bmaptool to flash wic image.

IMAGE=fsl-image-multimedia-full-imx8mqevk-20181018224131.rootfs.wic
DEVICE=/dev/sdb # The device may change in your system
sudo bmaptool copy $IMAGE $DEVICE --nobmap

 

0 Kudos
Reply