SDR104 support in USDHC2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDR104 support in USDHC2

1,229 Views
yashavanthashet
Contributor V

Hi,

 

We are using i.MX8M custom board with Linux4.9.51_ga release.

We are facing issue with UHS sd cards.

Even after removing "sd-uhs-sdr104" property from "&usdhc2" node in dts, card will detect with UHS SDR104 mode and fails. Kindly let us know where exactly we needs to change in order to make card detect only n DDR50 mode.

Thanks in advance.

Regards,

Yashavantha

4 Replies

868 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yashavantha

"sd-uhs-sdr104" property is not supported by i.MX8M usdhc driver

fsl-imx8mq.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

one can try "no-1-8-v", like:

&usdhc { ..
        no-1-8-v;
        status = "okay";

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

868 Views
yashavanthashet
Contributor V

Hi Igor,

What do u mean by ""sd-uhs-sdr104" property is not supported by i.MX8M"? Can't we test ultra high speed cards in i.MX8M board?

Then what is the maximum SD speed supported?

Thanks and Regards,

Yashavantha

0 Kudos

868 Views
igorpadykov
NXP Employee
NXP Employee

"sd-uhs-sdr104" property is optional and not supported by i.MX8M esdhc driver

linux/drivers/mmc/host/sdhci-esdhc-imx.c

sdhci-esdhc-imx.c\host\mmc\drivers - linux-imx - i.MX Linux kernel 

What is supported is documented on

linux/Documentation/devicetree/bindings/mmc/fsl-imx-esdhc.txt

fsl-imx-esdhc.txt\mmc\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

Supported speeds are described in sect.10.3.1.1 Features i.MX8M Reference Manual.

Best regards
igor

868 Views
yashavanthashet
Contributor V

Hi,

Any answer?

Thanks and Regardsm

Yashavantha

0 Kudos