SDP additional green board schematic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDP additional green board schematic

Jump to solution
2,189 Views
ko-hey
Senior Contributor II

Hi all

Do you have a newest SDP schematics ?


I bought a new SABRE-SDP and  see a schematic.However, there are some difference between a board that I bought and schematic.

The board are added green color boards that is shown in attachment in CSI I/F

.IMG_2574.jpg


Does someone have a schematic for additional boards ?



Ko-hey

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,047 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

seems this additional board is SPF-27820_A IMX6SDPCAMADP

(to get camera 90 deg rotated). Suggest to enter support ticket

to obtain its schematic.

Latest SABRE-SDP designfiles:

i.MX6_SABRE_SDP_DESIGNFILES : Design files, including hardware schematics, Gerbers, and OrCAD files..

Size (K): 11725 Format: zip Rev #: C4 Modified: 10/15/2014

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
2,048 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

seems this additional board is SPF-27820_A IMX6SDPCAMADP

(to get camera 90 deg rotated). Suggest to enter support ticket

to obtain its schematic.

Latest SABRE-SDP designfiles:

i.MX6_SABRE_SDP_DESIGNFILES : Design files, including hardware schematics, Gerbers, and OrCAD files..

Size (K): 11725 Format: zip Rev #: C4 Modified: 10/15/2014

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,048 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for your reply.

I have another question.

According to the latest schematic, MIPI CMOS Sensor is OV5640 and Parallel CMOS Sensor is OV5642.

However, the board that I bought had two OV5640 for both MIPI and Parallel.

Is these inclusions for SDP correct ?

Is the sensor changed ?

Ko-hey

0 Kudos
Reply
2,048 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

you can look at BOM file for included parts,

suggest to apply to local marketing for differencies.

Best regards

igor

2,048 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you.

I'll ask local marketing.

Ko-hey

0 Kudos
Reply