SDMA DMA Request numbers for IMX6Solox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDMA DMA Request numbers for IMX6Solox

1,292件の閲覧回数
niranjanbc
Contributor IV

Hi where can i find the dma request number for configuring Uart 5 RX/TX transfer using DMA on M4.

where are these request number specified in datasheet.

ラベル(7)
2 返答(返信)

1,135件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi niranjanbc

please refer to Table 3-3. SDMA event mapping i.MX6SoloX Applications Processor Reference Manual 

http://www.nxp.com/docs/en/reference-manual/IMX6SXRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,135件の閲覧回数
niranjanbc
Contributor IV

Got it Thanks  Igor

0 件の賞賛
返信