Objectives is the get the ENET driver up and running.
1. I have an SABRE SD board rev c with an imx6DL
2. I've built the platform SDK with the Sourcery toolchain , ./tools/build_sdk -clean -t mx6sdl -b smart_device -v c
3. I've run the ping.elf
4. The Link come up
Now here is the porblem
5. I can't see any frames getting sent, it looks like the first thing that happens is that lwIP sends an ARP, but I fail to see that on wireshark
and my laptop from which I try to ping the SabreSD say destination is unreachable.
I've build the LTIB U-boot. From there ping works fine.
WHat can be wrong in the SDK ENET driver?
regards
Andreas
解決済! 解決策の投稿を見る。
I've got it working using static IP, change the ping code to use static.
The issues were, due to using a 100Mbit switch I triggered 2 SDK issues.
enet_drv.c
1. The link status prints use a faulty mask.
if (((value>>14)&0x3) == 0x2)
dev->status |= ENET_STATUS_1000M;
else if (((value>>14)&0x3) == 0x2) <- Should be 0x1
dev->status |= ENET_STATUS_100M;
2. It is only configured for 1000M
dev->enet_reg->ECR.U |= ENET_ETHER_EN | ENET_ETHER_SPEED_1000M | ENET_ETHER_LITTLE_ENDIAN;
I guess the MAC should use the PHY negotiated speed?
regards
Andreas
Please connect the i.MX6 board to a router, the ping test requires DHCP.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I've got it working using static IP, change the ping code to use static.
The issues were, due to using a 100Mbit switch I triggered 2 SDK issues.
enet_drv.c
1. The link status prints use a faulty mask.
if (((value>>14)&0x3) == 0x2)
dev->status |= ENET_STATUS_1000M;
else if (((value>>14)&0x3) == 0x2) <- Should be 0x1
dev->status |= ENET_STATUS_100M;
2. It is only configured for 1000M
dev->enet_reg->ECR.U |= ENET_ETHER_EN | ENET_ETHER_SPEED_1000M | ENET_ETHER_LITTLE_ENDIAN;
I guess the MAC should use the PHY negotiated speed?
regards
Andreas
For some reason it reports 10M bps when it should be 100M bps. I cant verify the output since it seems impossible to find the AR8031 manual online.
Any clues?
ENET AR8031 PHY: ID=4dd070
enet phy status 1: 796d
AR8031 reg 0x11 = 7c1c
ENET 1: [ FULL_DUPLEX ] [ connected ] [ 10M bps ]: