SDK for SDMA functionality on IMX8MQ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK for SDMA functionality on IMX8MQ

1,322 次查看
vaparikh
Contributor II

I am working on the EVK-MIMX8MQ. I would like to use the SDMA functionality on the IMX8MQ but do not see any SDMA files in the driver folder. I see that the the IMX8MM has the SDK for SDMA. Could someone (preferably from NXP) please share the SDK for the IMX8MQ SDMA and ECSPI_SDMA? When can we expect to see it as a part of the online driver download?

1 回复

1,116 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

As you already mentioned, the SDMA driver is included on the SDK for i.MX8M Mini but is not available on the SDK for i.MX8MQ. There are not public plans about possible integration of this on future SDK releases for i.MX8MQ. In case of requiring this feature, you could request it on NXP Professional Services or discussing it with your assigned FAE.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------