SDIO transfer modes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDIO transfer modes

1,082 Views
syuriks
Contributor I

Hello,

Is SPI bus mode supported in SDIO host controller for data transfer in iMx8 processors? We're currently in stage of board design and we need separate pins for input/output for SDIO. As far as I could understand only SPI transfer mode supports this.

Thanks in advance

Yuri

0 Kudos
Reply
1 Reply

993 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuri

unfortunately it is not supported (usdhc module is the same on i.MX8 processors)

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply