SDIO SUPPORT on IMX8MM MINI LPD4-CPU2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDIO SUPPORT on IMX8MM MINI LPD4-CPU2

1,400 Views
vinayharitsakp1
Contributor III

Team,

I am trying to connect uSD Adapter Fixed 3.3 V rev A board to micro SD slot of IMX8MM MINI LPD4-CPU2. on the muratha board i am connecting CYW54591.

 

Following are the DTS changes i am doing

&usdhc2{

compatible = "fsl,imx6q-usdhc";
reg = <0x02194000 0x4000>;
interrupts = <0 23 0x04>;
clocks = <&clks 164>, <&clks 164>, <&clks 164>;
clock-names = "ipg", "ahb", "per";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc2_1>;
cd-gpios = <&gpio2 2 0>;
wp-gpios = <&gpio2 3 0>;
bus-width = <8>;
no-1-8-v;
non-removable;
mmc-pwrseq = <&usdhc2_pwrseq>;
pm-ignore-notify;
cap-power-off-card;
// keep-power-in-suspend;
enable-sdio-wakeup;
mmc-hs200-1_8v;
mmc-hs400-1_8v;
bus-width = <8>;
status = "okay";


brcmf: bcrmf@1 {
reg = <1>;
compatible = "brcm,bcm4329-fmac";
};
};

 

I am getting the following error message:

[ 43.332028] mmc1: sdhci: ADMA Err: 0x00000000 | ADMA Ptr: 0x00000000
[ 43.338468] mmc1: sdhci-esdhc-imx: ========= ESDHC IMX DEBUG STATUS DUMP =========
[ 43.346037] mmc1: sdhci-esdhc-imx: cmd debug status: 0x2180
[ 43.351695] mmc1: sdhci-esdhc-imx: data debug status: 0x2200
[ 43.357440] mmc1: sdhci-esdhc-imx: trans debug status: 0x2300
[ 43.363273] mmc1: sdhci-esdhc-imx: dma debug status: 0x2400
[ 43.368932] mmc1: sdhci-esdhc-imx: adma debug status: 0x2500
[ 43.374678] mmc1: sdhci-esdhc-imx: fifo debug status: 0x2680
[ 43.380424] mmc1: sdhci-esdhc-imx: async fifo debug status: 0x2750
[ 43.386689] mmc1: sdhci: ============================================
[ 53.471645] mmc1: Timeout waiting for hardware cmd interrupt.
[ 53.477404] mmc1: sdhci: ============ SDHCI REGISTER DUMP ===========
[ 53.483847] mmc1: sdhci: Sys addr: 0x00000000 | Version: 0x00000002
[ 53.490286] mmc1: sdhci: Blk size: 0x00000000 | Blk cnt: 0x00000001
[ 53.496725] mmc1: sdhci: Argument: 0x00000000 | Trn mode: 0x00000000
[ 53.503165] mmc1: sdhci: Present: 0x00688009 | Host ctl: 0x00000001
[ 53.509605] mmc1: sdhci: Power: 0x00000000 | Blk gap: 0x00000080
[ 53.516045] mmc1: sdhci: Wake-up: 0x00000008 | Clock: 0x000010ff
[ 53.522486] mmc1: sdhci: Timeout: 0x0000008e | Int stat: 0x00000000
[ 53.528927] mmc1: sdhci: Int enab: 0x007f1003 | Sig enab: 0x007f1003
[ 53.535367] mmc1: sdhci: ACmd stat: 0x00000000 | Slot int: 0x00000502
[ 53.541808] mmc1: sdhci: Caps: 0x07eb0000 | Caps_1: 0x8000b407
[ 53.548249] mmc1: sdhci: Cmd: 0x00000502 | Max curr: 0x00ffffff
[ 53.554688] mmc1: sdhci: Resp[0]: 0x00000000 | Resp[1]: 0x00000000
[ 53.561126] mmc1: sdhci: Resp[2]: 0x00000000 | Resp[3]: 0x00000000
[ 53.567566] mmc1: sdhci: Host ctl2: 0x00000000
[ 53.572010] mmc1: sdhci: ADMA Err: 0x00000000 | ADMA Ptr: 0x00000000
[ 53.578450] mmc1: sdhci-esdhc-imx: ========= ESDHC IMX DEBUG STATUS DUMP =========
[ 53.586019] mmc1: sdhci-esdhc-imx: cmd debug status: 0x2180
[ 53.591676] mmc1: sdhci-esdhc-imx: data debug status: 0x2200
[ 53.597422] mmc1: sdhci-esdhc-imx: trans debug status: 0x2300
[ 53.603254] mmc1: sdhci-esdhc-imx: dma debug status: 0x2400
[ 53.608913] mmc1: sdhci-esdhc-imx: adma debug status: 0x2500
[ 53.614659] mmc1: sdhci-esdhc-imx: fifo debug status: 0x2680
[ 53.620407] mmc1: sdhci-esdhc-imx: async fifo debug status: 0x2750

Request you to guide me if the MicroSD slot on Imx8mm mini  evk board supports sdmmc/ reconfiguration of SDIO.

0 Kudos
Reply
5 Replies

1,273 Views
vinayharitsakp1
Contributor III

Team,

Do We have any update on the ticket? 

@sdio, imx8m mini, cyw4373, wifi, bt

0 Kudos
Reply

1,325 Views
vinayharitsakp1
Contributor III

Team, Please clarify the same. A faster resolution of the ticket would help me.

I am using I. MX 8M MINI : 8MMINILPD4-CPU2 :: 8MM MINI :BB Board.

The version of Board i can see behind the board i am using  is SCH-31407 REV C4 and bar code number TR21250978.

Can we connect murata uSD-M.2 to SD card slot of iMX8M Mini EVK Board?

Will usdhc2 work on this SD card slot on iMX8MM mini?

if usdhc2 works on SD card slot on the above mentioned board then .please suggest the changes i need to incorporate.

0 Kudos
Reply

1,252 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The uSDHC1 and uSDHC2 of EVK board is connected to WIFI and MicrosSD card
slot respectively. So just use the uSDHC1 for wifi, uSDHC2 is used for SD CARD.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enabling-uSDHC1-of-i-MX8MM-Based-On-L5-4...

0 Kudos
Reply

1,338 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For the i.MX8MM evk BOARD are you using the old version or newest version Board?

0 Kudos
Reply

1,335 Views
vinayharitsakp1
Contributor III

Team,

I am using I. MX 8M MINI : 8MMINILPD4-CPU2 :: 8MM MINI :BB Board.

The version of Board i can see behind the board i am using  is SCH-31407 REV C4 and bar code number TR21250978

0 Kudos
Reply