SD2_CLK not detected in mx53 based design with customized R10.4 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SD2_CLK not detected in mx53 based design with customized R10.4 BSP

931件の閲覧回数
Mats1z
Contributor III

My board is based on mx53_smd ref design. A WLAN module is connected to SD2 interface. It is detected as SDIO device. This SD2 is configured without card detection. It is configured as mmc2 device and card_inserted_state is hardcoded as 1 in mxc_mmc_platform_data mmc2 structure.

Now I'm unable to detect the SD2_CLK . I have made no other changes in the BSP regarding this section.

Is it the driver that should load the device? Then only the CLK will be provided??

Please share your thoughts

ラベル(3)
タグ(5)
0 件の賞賛
返信
0 返答(返信)