SD images and cross-complation repos

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD images and cross-complation repos

1,725 Views
molin_du
Contributor II

Hello I am new to NXP i.MX8 and Yocto.

Does NXP provide a repo warehouse or git where all available SD images and correponding cross-complation enviroment stored?

current I have a 4.9.88 SD image but I don't have cross-compile enviroment, also I would like to add Qt and OpenCV to my system.

Best 

Tags (2)
3 Replies

1,642 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Molin,

You can download the demo image that include the sd images, also include the one for QT that include openCV, You can download it from:

Embedded Linux for i.MX Applications Processors | NXP 

Regards

0 Kudos
Reply

1,642 Views
molin_du
Contributor II

Hello Bio:

Thank you for reply.

I found the SD images and I downloaded 5.4 xxx, burn and run it successful.

what I need is its cross-compilation enviroment to compose my own app. 

currently there is no header, and compiler inside this bare Linux SDImage.

Best,

1,642 Views
molin_du
Contributor II

Hello:

finally I got a non perfect solution,

   I unzip SD image files to my host machine to have all *.so collected.

  and I download source of my interest packages, such as opencv, etc, put the header files in corresponding folder

therefore I somehow can cross-compile and the output is runnable at i.MX8 QXPMEK