SD card image of IMXEBOOKDC3-E (E-ink panel)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD card image of IMXEBOOKDC3-E (E-ink panel)

Jump to solution
1,000 Views
torus1000
Contributor V

Hi,

I accidentally crashed my bundled SD card which attached to the IMXEBOOKDC3-E (E-ink panel for MX6SL-EVK) and I don't have any backup of it.

Where can I download the SD card image labeled "MX6SLEVK-E-INK ANDROID r12.10.02"?

Is it exactly same demo image as KK442* or L500** except bootargs*** ?

where

  * KK442: https://www.nxp.com/webapp/Download?colCode=KK442_100_ANDROID_DEMO_EVK_BSP

  ** L500: https://www.nxp.com/webapp/Download?colCode=IMX6-L500-100-DEMO-EVK-BSP

  *** bootargs: video=mxcepdcfb:E060SCM,bpp=16 max17135:pass=2,vcom=-2030000

Can anybody help me?

BR

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
708 Views
b36401
NXP Employee
NXP Employee

I placed my Android SD card image for iMX6SL EVK with E-INK here:

http://photo.afti.ru/tmp/fs/imx6sl-evk-eink-android.image.gz

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
709 Views
b36401
NXP Employee
NXP Employee

I placed my Android SD card image for iMX6SL EVK with E-INK here:

http://photo.afti.ru/tmp/fs/imx6sl-evk-eink-android.image.gz

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
708 Views
torus1000
Contributor V

I found following thread.

Kitkat support for EPD in i.mx6slevk

https://freescale.jiveon.com/thread/334197

The latest Android BSP that supported the i.MX6SL EPD is Android Ice Cream Sandwich (R13.5).

So I will try this later.

Demo Image Flashed on the i.MX 6SoloLite EVK SD Cards (REV R13.5)  ZIP  (1.6 GB) 11/9/2012

https://www.nxp.com/webapp/Download?colCode=IMX6_SL_SDP_SD_DEMO_IMAGE

0 Kudos
Reply