SD card configuration on i.Mx7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD card configuration on i.Mx7D

2,021 Views
sharmilad
Contributor I

Hi,

     We are using i.Mx7Dual processor for one of our custom product. We are planning to use SD card for storage purpose. I have configured usdhc in kernel device tree as shown below, I have kept the same configuration in uboot but in uboot sd card is detecting and I am getting the output as shown below .

=> mmc info
Device: FSL_SDHC
Manufacturer ID: 12
OEM: 3456
Name: SDBus Speed: 25000000
Mode : SD Legacy
Rd Block Len: 512
SD version 1.0
High Capacity: Yes
Capacity: 14.8 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes 

The dts file:

&usdhc2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc2>;
cd-gpios = <&gpio5 9 GPIO_ACTIVE_LOW>;
vmmc-supply = <&reg_sd2_vmmc>;
tuning-step = <2>;
bus-width = <4>;
no-1-8-v;
status = "okay";
};

pinctrl_usdhc2: usdhc2grp { // SD card
fsl,pins = <
MX7D_PAD_SD2_CMD__SD2_CMD 0x59
MX7D_PAD_SD2_CLK__SD2_CLK 0x19
MX7D_PAD_SD2_DATA0__SD2_DATA0 0x59
MX7D_PAD_SD2_DATA1__SD2_DATA1 0x59
MX7D_PAD_SD2_DATA2__SD2_DATA2 0x59
MX7D_PAD_SD2_DATA3__SD2_DATA3 0x59
MX7D_PAD_SD2_CD_B__GPIO5_IO9 0x59
>;
};

But in kernel SD card is not detecting. I have added prints in the drivers and find out that driver is failing at mmc_send_app_op_cond() function. 

Please help me to resolve the issue.

Thanks & Regards,

Sharmila D

0 Kudos
Reply
7 Replies

2,004 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @sharmilad 

I have identified few changes in pin-mux(Modify the Drive strength). Please change the code like below.

MX7D_PAD_SD2_CMD__SD2_CMD 0x59
MX7D_PAD_SD2_CLK__SD2_CLK 0x19
MX7D_PAD_SD2_DATA0__SD2_DATA0 0x59
MX7D_PAD_SD2_DATA1__SD2_DATA1 0x59
MX7D_PAD_SD2_DATA2__SD2_DATA2 0x59
MX7D_PAD_SD2_DATA3__SD2_DATA3 0x59

Modify the alias like below.

mmc0 = &usdhc1;
mmc1 = &usdhc2;
mmc2 = &usdhc3;

Thanks & Regards

Sanket Parekh

0 Kudos
Reply

1,999 Views
sharmilad
Contributor I

 

Hi,

    I have tried the above changes but I didn't  help.I am attaching dmesg Log FYR.

Thanks & Regards,

Sharmila

0 Kudos
Reply

1,994 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @sharmilad 

Can you please share schematic portion of SD card with microprocessor?

Thanks & Regards

Sanket Parekh

0 Kudos
Reply

1,984 Views
sharmilad
Contributor I

Attaching the files.

For an update, We have populated R441 and removed R425.

0 Kudos
Reply

1,965 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @sharmilad 

SD2_CD_B pin is active low pin, for card detection SD2_CD_B pin should be in low state. Is this SD2_CD_B pin going low? Can you check the same with the help of DMM?

Thanks & Regards

Sanket Parekh

0 Kudos
Reply

2,015 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @sharmilad 

I hope you are doing well.

Please remove line "tuning-step = <2>;" and share the dmesg logs and board DTS file.

Thanks & Regards

Sanket Parekh

0 Kudos
Reply

2,011 Views
sharmilad
Contributor I

Hi,

I have tried removing that line but that didn't help. I am attaching my dmesg and dts file.

Thanks & Regards,

Sharmila

Tags (1)
0 Kudos
Reply