SD card boot problem when LCD and USB both attached

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SD card boot problem when LCD and USB both attached

2,483 次查看
fcs
Contributor IV

I have noticed that typically when I have our LVDS LCD screen plugged in (not necessarily with boot args configured to use it) and USB devices plugged in (keyboard & mouse or even just one of them), the bootup of the QSB demo SD card usually/always fails with the following error:

 

Waiting for root device /dev/mmcblk0p1...

usb 1-1.1: new low speed USB device using fsl-ehci and address 3

input: Microsoft Microsoft 3-Button Mouse with IntelliEye(TM) as /devices/platform/fsl-ehci.0/usb1/1-1/1-1.1/1-1.1:1.0/input/input5

generic-usb 0003:045E:0040.0001: input: USB HID v1.10 Mouse [Microsoft Microsoft 3-Button Mouse with IntelliEye(TM)] on usb-fsl-ehci.0-1.1/input0

usb 1-1.2: new low speed USB device using fsl-ehci and address 4

input: Dell Dell USB Keyboard as /devices/platform/fsl-ehci.0/usb1/1-1/1-1.2/1-1.2:1.0/input/input6

generic-usb 0003:413C:2003.0002: input: USB HID v1.10 Keyboard [Dell Dell USB Keyboard] on usb-fsl-ehci.0-1.2/input0

mmc0: error -110 whilst initialising SD card

 

The complete log is attached.

 

Without a USB device plugged in, the bootup is fine, after which the USB devices can be plugged in and work.

 

The problem is arising in here somewhere, err -110 means "ETIMEDOUT       110     /* Connection timed out */":

 

/*
* Starting point for SD card init.
*/
int mmc_attach_sd(struct mmc_host *host, u32 ocr)
{
        int err;

        BUG_ON(!host);
        WARN_ON(!host->claimed);

        mmc_sd_attach_bus_ops(host);

        /*
         * We need to get OCR a different way for SPI.
         */
        if (mmc_host_is_spi(host)) {
                mmc_go_idle(host);

                err = mmc_spi_read_ocr(host, 0, &ocr);
                if (err)
                        goto err;
        }

        /*
         * Sanity check the voltages that the card claims to
         * support.

         */
        if (ocr & 0x7F) {
                printk(KERN_WARNING "%s: card claims to support voltages "
                       "below the defined range. These will be ignored.\n",
                       mmc_hostname(host));
                ocr &= ~0x7F;
        }

        if (ocr & MMC_VDD_165_195) {
                printk(KERN_WARNING "%s: SD card claims to support the "
                       "incompletely defined 'low voltage range'. This "
                       "will be ignored.\n", mmc_hostname(host));
                ocr &= ~MMC_VDD_165_195;
        }

        host->ocr = mmc_select_voltage(host, ocr);

        /*
         * Can we support the voltage(s) of the card(s)?
         */
        if (!host->ocr) {
                err = -EINVAL;
                goto err;
        }

        /*

        * Detect and init the card.
         */
        err = mmc_sd_init_card(host, host->ocr, NULL);
        if (err)
                goto err;

        mmc_release_host(host);

        err = mmc_add_card(host->card);
        if (err)
                goto remove_card;

        return 0;

remove_card:
        mmc_remove_card(host->card);
        host->card = NULL;
        mmc_claim_host(host);
err:
        mmc_detach_bus(host);
        mmc_release_host(host);

        printk(KERN_ERR "%s: error %d whilst initialising SD card\n",
                mmc_hostname(host), err);

        return err;

}

Original Attachment has been moved to: SD-card-error-that-happens-when-LCD-and-USB-attached.txt.zip

标签 (2)
标记 (6)
3 回复数

1,702 次查看
phuongdangminh
Contributor III

I have the same problem. Have you fix it yet ?

0 项奖励
回复

1,702 次查看
fcs
Contributor IV

No, it just happens less often now.

1,702 次查看
fcs
Contributor IV

It has something to do with excessive power consumption. The more devices you have plugged in (display, USB mouse etc) the more likely it is to happen.