SD card access in guest for imx6qsd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SD card access in guest for imx6qsd

908件の閲覧回数
prethibhas
Contributor I

Hi,

I'm trying to access sd card in guest using virtio block.I am able to start loading the guest by adding the DTS entry for virtio in both guest and hypervisor I use but getting stuck when trying to read partition details(msdos partition) from virtblk_probe(). I traced it and found that it is not returning from wait_on_page_read() in linux4.5/mm/filemap.c.

Can anyone suggest a solution..?

Regards,

Prethibha

ラベル(3)
0 件の賞賛
返信
1 返信

822件の閲覧回数
b36401
NXP Employee
NXP Employee

Please make sure that guested OS supports SDcard reader.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信