Hi
I am working on QWKS-SCMiMX6Q board for performance needed project. Right now I am evaluating the SCMiMX6Q using the qwks board with L4.1.15 kernel and krogoth release. For various reasons, we need to move SCMiMX6q against our own iMX6SOLO board. While evaluating the performance of SCMiMX6q we found it drastically lags in performance compared to our iMX6SOLO board. The test was conducted using the standard benchmark tools to analyze the performance of DDR. SCM is having a RAM of 1GB LPDDR and our iMX6SOLO is also having 1GB DDR3 RAM. Both processors operate on 32-bit mode and same DDR-Frequency of 400MHz.
BENCHMARK TOOLS used:
PERFORMANCE ANALYSIS:
LMBENCH was used to analyze LATENCY
MBW and STREAM were used to analyze BANDWIDTH
| LMBENCH | STREAM | MBW | |
|---|---|---|---|
| SCMiMX6Q | 57.240ns | 592.77 MB/sec | 274.556 MiB/s | 
| iMX6SOLO | 42.639ns  | 1104.97 MB/sec | 685.166 MiB/s | 
SCMiMX6Q is less than half speed of our iMX6SOLO board.
the Actual results must be SCMiMx6q should give more performance compared to SOLO.I suspect the performance is due to the mismatch of the clock frequency for mmdc controllers in SCM.
CLOCK:
mmdc_ch1_axi 528000000
mmdc_ch0_axi 396000000
Actual suggested frequency rate for DDR is 400 MHZ but why there is a difference. What is the reason behind huge performance difference in SCM.It will affect our products also.I am really running out of ideas.
Any Patches or fix for this issue
Hoping for a faster and better guidance
Hi Manoj
in general this may be explained by different burst size as described on
One can try to further analyze it with mmdc profiling described on above link
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------