SCFW API included in Linux Kernel 5.4.24?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCFW API included in Linux Kernel 5.4.24?

1,430件の閲覧回数
lorenzo_giraudi
Contributor III

Hello,

I see that inside the imx-scfw-porting-kit there is a scfw-export-linux folder with some APIs to be called by the kernel. What i don't understand is: do i need to move these files inside the linux-imx v5.4.24? Or are they already present?

For instance, what if i want to create/modify a partition for HW access?

ラベル(2)
0 件の賞賛
返信
1 返信

1,422件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello lorenzo,

 

They are already present, you can create a partition in hardware but not modifying these files since this file are just an api.

 

Regards