Hi
We currently have a development with an iMX6DL in production.
We plan on starting a new development that requires an interface to a SATA SSD now and potentially a NVMe in the future
According to the feature set https://www.nxp.com/docs/en/supporting-information/FLYRIMXPRDCMPR.pdf only the Plus range support SATA
However all the SabreSD eval boards include a SATA interface and the schematic indicates that they are wired to the Processor on both the Plus and non Plus devices.
There is also quite a bit of dicussion about SATA with respect to the iMX in these discussion pages
So I'm wondering if you could confirm if the Dual and DualLite both support SATA? Or is it exclusively the DualPlus?
Regards
Diarmuid
@diarmuidcollins
Hello,
please refer to the following:
https://community.nxp.com/t5/i-MX-Processors/i-MX6-SATA/m-p/739479
Regards,
Yuri.