SATA Speed is quite low at IMX6D platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SATA Speed is quite low at IMX6D platform

1,350 Views
houjunjie
Contributor I

Now we are using IMX6D platform and the kernal version of it is 4.1.15 to test SATA speed. The result of both Read and Write is only 67MB/s. And we tested the SSD in different ARM platform, the speed can achieve 500MB/s. This speed 67MB/s is even not meet SATA1.0.

Our project is quite urgent, please help to give us some advice. Thanks.

Junjie 

Labels (1)
0 Kudos
Reply
3 Replies

1,193 Views
igorpadykov
NXP Employee
NXP Employee

Hi Junjie 

reason may be signal integrity issues (noise), one can try to improve

signal shape using IOMUXC_GPR13 register described in sect.36.4.14 GPR (IOMUXC_GPR13)

i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Also one can recheck sata signal layout, using layout requirements provided in

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,193 Views
houjunjie
Contributor I

Hi Igor:

Actually our layout is totally same as your reference design. And also we tested the SATA speed in your EVB with kernal 4.1.15 and we got same issue. The EVB is as below. Please help to check it.微信图片_20180920100553.jpg

0 Kudos
Reply

1,193 Views
igorpadykov
NXP Employee
NXP Employee

Hi Junjie 

please check

iMX6Q SATA performance (speed limit) 

Best regards
igor

0 Kudos
Reply