SAI features ( Time Stamping and Bit Count) in i.MX8M Mini

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SAI features ( Time Stamping and Bit Count) in i.MX8M Mini

1,056 次查看
nxa14910
NXP Pro Support
NXP Pro Support

The i.MX8M Mini SAI peripheral has two features that other processors with an SAI interface do not have (eg i.MX RT 1064), and therefore the low level driver in the SDK does not support them. Is there any documentation that describes what these features are and how they are used?

Thank You

Doug Bruce

标签 (1)
2 回复数

982 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Doug Bruce,


Besides the Reference Manual, which as Karan Gajja mentioned is a good starting place, I would also recommend checking the i.MX Linux Reference Manual (part of the Linux BSP documentation) for more information about the Linux Driver, which may provide some help.


Regards,

982 次查看
karangajjar
Senior Contributor II

Hi Doug Bruce,

Have you checked out the i.MX8M mini Reference Manual? Please see below link for more details. It has information regarding Time stamping and Bit count and also their registers.

https://www.nxp.com/webapp/Download?colCode=IMX8MMRM 

Regards,
Karan Gajjar

0 项奖励
回复