SABRESD ubuntu 14.04 Xorg driver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRESD ubuntu 14.04 Xorg driver?

1,444 Views
c2h2
Contributor II

Hi, I am using SABRESD fsl kernel 3.10.17 ubuntu 14.04, I have installed xfce desktop, but my 1080p HDMI screen is very laggy. I noticed that Xorg driver is not built. wondering how to compile this?

Labels (2)
0 Kudos
6 Replies

670 Views
c2h2
Contributor II

This must be a way to build it.

0 Kudos

670 Views
jamesbone
NXP TechSupport
NXP TechSupport

Bio_TICFSL,  is this available?

0 Kudos

670 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

I guess Xorg is not used by 14.04, however please check is the packaged is installed in your system

ps ax | grep `pgrep Xorg` | head -1

And this executable is provided by the xserver-xorg binary package

$ pkg -S /usr/bin/X

xserver-xorg: /usr/bin/X

Please check;

https://community.freescale.com/docs/DOC-100626

Instead of xorg, as option you should try wayland

http://wayland.freedesktop.org/

0 Kudos

670 Views
EricNelson
Senior Contributor II

Hello Bio_TICFSL,

DOC-100626 has nothing to do with running Trusty on the SABRE-SD. It's related to using Trusty (14.04) as a build machine with LTIB.

We've also been investigating getting the Vivante drivers working on Trusty, and there are some differences from Saucy and earlier releases. We think it has to do with Xorg version 1.15, but don't have many details yet.

0 Kudos

670 Views
OtavioSalvador
Senior Contributor II

Yes EricNelson, the Xorg 1.15 is not supported in 3.10.17 GA drivers. This is supported only with 3.10.31 Alpha release one.

You need to keep Xorg 1.14 to Ubuntu 14.04 to use 4.9.6p13 Vivante drivers.    

0 Kudos

670 Views
EricNelson
Senior Contributor II

Thanks Otavio.

0 Kudos