SABRESD ubuntu 14.04 SD booted, HOWTO access eMMC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRESD ubuntu 14.04 SD booted, HOWTO access eMMC?

Jump to solution
4,678 Views
c2h2
Contributor II

Hi all,

Following i.MX6q SABRE Board for Smart Devices - Linux on ARM - eewiki guide. I have successfully installed ubuntu 14.04 into my Freescale SABRESD demo board. Everything is running, but I don't see the on-board eMMC device in my /dev/mmcblk* list and `lsblk` didn't show either, only storage device I can see is my SD card. Can someone tell me how to access the EMMC device?

Thanks!

Labels (3)
0 Kudos
Reply
1 Solution
3,852 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuling

I did not try eewiki, but on Freescale BSP releases

eMMC is "mmcblk0" - actually what is mentioned on eewiki.

You can try with Freescale kernel below and check

L3.10.17_1.0.0_IMX6QDLS_BUNDLE

L3.10.17_1.0.0_LINUX_DOCS

Best regards

chip

View solution in original post

0 Kudos
Reply
5 Replies
3,852 Views
c2h2
Contributor II

This is resolved by using official kernel L3.10.17_1.0.0_IMX6QDLS_BUNDLE

3,852 Views
yangjiao
Contributor I

Hi Yiling,

I am trying to install ubuntu 14.04 to emmc about imx6q sabresd board..follow the i.MX6q SABRE Board for Smart Devices - Linux on ARM - eewiki .

How can you tell me how you are install?

你好,我也正在安装ubuntu14.04在这个imx6q sabresd板子上,开始也是按照eewiki的教程安装在SD卡上没问题。请教你是怎么把ubuntu14.04安装到emmc中的呢?我安装了好几天了,用Mfgtool烧写,但是uboot就是挂载不上内核,很郁闷。

向您请教

在线等

0 Kudos
Reply
3,852 Views
gusarambula
NXP TechSupport
NXP TechSupport

There was another thread that was vaguely similar in which the Block Devices were not enabled and this was causing the eMMC not to be recognized. It might be of help:

https://community.freescale.com/thread/320241

0 Kudos
Reply
3,853 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuling

I did not try eewiki, but on Freescale BSP releases

eMMC is "mmcblk0" - actually what is mentioned on eewiki.

You can try with Freescale kernel below and check

L3.10.17_1.0.0_IMX6QDLS_BUNDLE

L3.10.17_1.0.0_LINUX_DOCS

Best regards

chip

0 Kudos
Reply
3,852 Views
c2h2
Contributor II

Thanks for your reply, I will give a try, so if successful, what I am expected to see is that, I will have both /dev/mmcblk0* and /dev/mmcblk1* ? Thanks!

0 Kudos
Reply