Hi,
I want to connect an M.2 SATA SSD to the SABRESD board. To do this it appears that I need to use a 22-pin SATA to M.2 adapter. Can I use something like this?
https://www.amazon.co.uk/2-5inch-Adapter-Based-Converter-Card/dp/B08FCZ75M1/
Specifically, will this physically fit ok, as there doesn't appear to be a whole lot of clearance around the 22-pin connector on the board?
Thanks,
Alan
>Which i.MX series are you using? The i.mx6q/qp can support SSD device via sata interface
I'm using the i.MX6QP.
Yes I understood that this processor can support an SSD device via the 22-pin SATA connector.
My question was about how to connect the SSD to the board.
In the meantime I have ordered a 22-bin SATA cable which I believe is the answer to my original question. If not I will follow up with further questions once it arrives and I have a chance to test it.