SABRE SD. SATA and HDMI together

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE SD. SATA and HDMI together

Jump to solution
1,201 Views
dmitriykornoush
Contributor III

Hello to All

I use SABRE SD board.

Hdd connected to SATA port, monitor to HDMI.

If I plug monitor and HDD together, monitor is work good, SATA HDD not viewed (linux write NO SATA DISK during boot)

If I connect only SATA HDD during boot, and connect HDMI after boot, all work fine.

If I comment

imx6q_add_mxc_hdmi_core(&hdmi_core_data);

imx6q_add_mxc_hdmi(&hdmi_data);

in board-mx6q-sabresd.c

device boot and only SATA work.

How to solve this problem?

Labels (1)
0 Kudos
Reply
1 Solution
1,018 Views
dmitriykornoush
Contributor III

Problem solved. Solution: switch power on to the SATA in u-boot, i.e. early that core booted

View solution in original post

1 Reply
1,019 Views
dmitriykornoush
Contributor III

Problem solved. Solution: switch power on to the SATA in u-boot, i.e. early that core booted