SABRE SD Board Altium layout files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE SD Board Altium layout files

Jump to solution
1,323 Views
Jochi119
Contributor II

Hello,

Does anyone have the converted .brd files for Altium on the layout files for the SABRE SDB? I only have a free version of Altium and can't import the .brd files

Thanks Joseph

0 Kudos
1 Solution
1,003 Views
Yuri
NXP Employee
NXP Employee

Please try import (not open) option of Altium.  Say, the files ".alg" usually are used to transfer

PCB design data to Altium. You may find some examples on the Community for i.MX6.

Regards,

Yuri.

View solution in original post

0 Kudos
3 Replies
1,003 Views
Yuri
NXP Employee
NXP Employee



 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,003 Views
Jochi119
Contributor II

Hey Yuri,

I cant open these files because I don't have OrCad.  Is there a way that you can convert them to Altium files for me?

Thank you

0 Kudos
1,004 Views
Yuri
NXP Employee
NXP Employee

Please try import (not open) option of Altium.  Say, the files ".alg" usually are used to transfer

PCB design data to Altium. You may find some examples on the Community for i.MX6.

Regards,

Yuri.

0 Kudos