SABRE Platform for Smart Devices, i.MX6DL. Four touch keys on the bottom of the touch screen didn't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE Platform for Smart Devices, i.MX6DL. Four touch keys on the bottom of the touch screen didn't work

1,554 Views
刚赵
Contributor I

The board I bought from the official website is SABRE Platform for Smart

Devices, i.MX6DL. When I run android 4.4.3 using i.mx6 BSP ,I found four

touch keys on the bottom of the touch screen didn't work. How can I use

these keys. I geussed the four keys are "home", "menu", "return" and

"search". Attachment is the photo of the keys on board(or on screen).

01129640108227_IMG_0711.JPG

0 Kudos
2 Replies

1,456 Views
maitegonzalez
Contributor I

Hii!

I have received the sabre plaftorm and I have the same problem described above.. I used the Default given SD.. Any suggestions?  I have only one board so I cant test if it has some hardware problem..

Thankss!!

Maite

0 Kudos

1,456 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi 刚,

Here you boot up the board with the Default given SD card with Demo images? Or you build images yourself? If you are using the default given device, have you tried another board to make sure if is the hardware problem?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos