SABRE Platform for Smart Devices Hardware Files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SABRE Platform for Smart Devices Hardware Files

跳至解决方案
1,695 次查看
mariuszlacina
Contributor II

I'm looking for hardware design files of the SABRE-SDP board (MCIMX6DL-SDP). Provided links doesn't work.

1 解答
1,609 次查看
samsaprunoff
Contributor V
4 回复数
1,610 次查看
samsaprunoff
Contributor V
1,609 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Thank you Sam, for sharing the link!

Maruisz, let us know if you have problems downloading the files from that link. It is most likely that you will need to login in order to download the files.

Regards,

0 项奖励
回复
1,609 次查看
mariuszlacina
Contributor II

I was able to download it. Thanks a lot !

Best regards

Mariusz

0 项奖励
回复
1,609 次查看
RossMcLuckie
NXP Employee
NXP Employee

Hi,

The SABRE Platform is being discontinued, which may explain why you can't access the files. Depending on your needs you can use the SABRE Board files.

The Platform and Board are the same PCB, just a different BOM / build option, with the Platform being a fully populated more expensive solution, the Board is a smaller BOM and cheaper overall solution.

You can access the Quad SABRE Board files here -

i.MX 6Quad SABRE Development Board|NXP 

Again this is the same PCB as used on the Dual versions. AFAIK an updated Dual SABRE Board is being created to replace the Dual SABRE Platform, but that will not be available until early next year.

Regards

Ross