SABRE Platform for Smart Devices Based on the i.MX 6 series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE Platform for Smart Devices Based on the i.MX 6 series

1,299 Views
jeffreycollins
Contributor II

I plugged in this board with the expectation that it would boot off the included SD card and I would see android on the included display. The display shows nothing, nothing comes out the speakers and the FDI driver for Win7 does not work. Are there any tips or instructions to get this thing working out of the box?

Labels (3)
0 Kudos
Reply
2 Replies

1,177 Views
jeffreycollins
Contributor II

Turns out on both boards I purchased, the LVDS cables were unplugged. They do not have locking connectors, they are friction fit only. I had to slide the units out of the plastic case reconnect the cables and carefully slide it back into the case. It is kind of a snug fit, and took several tries before I could reassemble the unit without inadvertantly having the LVDS cable slide out of the connector.