SABRE Platform for Smart Devices Based on the i.MX 6 series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SABRE Platform for Smart Devices Based on the i.MX 6 series

1,273 次查看
jeffreycollins
Contributor II

I plugged in this board with the expectation that it would boot off the included SD card and I would see android on the included display. The display shows nothing, nothing comes out the speakers and the FDI driver for Win7 does not work. Are there any tips or instructions to get this thing working out of the box?

标签 (3)
0 项奖励
回复
2 回复数

1,151 次查看
jeffreycollins
Contributor II

Turns out on both boards I purchased, the LVDS cables were unplugged. They do not have locking connectors, they are friction fit only. I had to slide the units out of the plastic case reconnect the cables and carefully slide it back into the case. It is kind of a snug fit, and took several tries before I could reassemble the unit without inadvertantly having the LVDS cable slide out of the connector.